This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请问TUSB8020的开发板实际测试时工作温度在多少?接线参考:上行口Type C,下行口:一个USB3.0设备,一个USB2.0设备。
产品:客户做的产品是眼球追踪模块,其中一种用途是放在VR头盔上使用,捕捉人眼球的动作。
客户问题以及现状:客户现在的主要问题是发热,工程师在样机测试的时候发现我们的TUBS8020发热较高,大概在50多度,因为这个板子是放在人眼附近的,所以这个温度太高,客户理想的温度是30-40度之间。
TUSB8020的最大结温能达105度,但是典型值为25度,在datasheet中7.3部分有介绍。
有没有将散热焊盘(thermal pad)接地来提高散热性能?
是的,25度是一个典型值,这个就是实验测得的结果,结温是可以按照热阻,功率来计算结温大小,Tj = Ta + Pd × theta Ja.
themal pad 是要尽量大面积的和GND Plane相连。
不好意思手头上没有这块demo板。
Kailyn,
按照理论值计算发热量不会达到50°这么高,这个问题仍然在处理中,我们仍然在找原因,谢谢你的解答。