This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913/914调试问题 无法建立连接

TI工程师,您好!

        调试DS90UB913/914遇到如下问题,烦请指导:

  

1. 单独914时I2c可正常读写,连上913后无法正常读写。

2. 测试LOCK始终为低电平。

3. BIST模式测试LOCK为低电平,PASS为如下波形

  • Gang Li,您好

    1. LOCK一直为底,有可能是硬件问题,请核对一下原理图和PCB,参考913A规格书40页和914A规格书48页的参考电路。

    2. 使用同轴电缆还是屏蔽双绞线?有没有使用同轴电缆输电?如果有输电,建议913先单独供电,看能否正常工作。

    3. 请问连上913后,能通过I2C正常读取914吗?

    4. 此时有没有视频信号发往913?

    谢谢!

    Kevin Zhang

  • 你好,我现在遇到的情况与Gang Li差不多,914端电路如上图(项目仅对913进行配置,不做视频解串)

    BIST脚置高,LOCK,PASS脚都输出为低电平

    1:使用同轴线.,并使用同轴线输电,检查913端供电正常(3.3V,1.8V)

    2:不管是否连上913,914端的RIN0都有一个同频反向的信号输出,且I2C对914的操作一切正常

    请问上图电路是否有问题,为何BIST=1,913接入与否,为何LOCK与PASS都低电平?

    测试条件如下:

    1:BIST=1

    2:OSS_SEL=1

    3:OEN=1

    4:MODE 10k上拉,0R下地

  • 你好,这个Lock为低的问题你最后解决了吗?是什么原因导致的