This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下DS90C385相应IC选型

Other Parts Discussed in Thread: AM3358, DS90C385A

您好!

      我最近在采用AM3358接10寸的彩色TFT,发现AM3358 输出的LCD接口为:RGB24bit,以及行,场同步,以及位时钟线等,而10寸屏基本上为LVDS接口,

DE MODE 物理接口, 我看到网上有的说采用DS90C385,因为不是很确定,故在此请教下,选用哪些IC较为合适?我的分辨率为 1280*800/60HZ,工作温度为

-10°-40°,谢谢。