Other Parts Discussed in Thread: AM3358, DS90C385A
您好!
我最近在采用AM3358接10寸的彩色TFT,发现AM3358 输出的LCD接口为:RGB24bit,以及行,场同步,以及位时钟线等,而10寸屏基本上为LVDS接口,
DE MODE 物理接口, 我看到网上有的说采用DS90C385,因为不是很确定,故在此请教下,选用哪些IC较为合适?我的分辨率为 1280*800/60HZ,工作温度为
-10°-40°,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,DS90C385可以满足你的要求,建议采用DS90C385A,是DS90C385的一个升级版本。
工作温度也符合要求,DS90C385A的工作温度范围为-10~70度。