This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
前端CMOS相机输出1412x876 50hz的视频,经过FPGA产生1024x768 50HZ视频(VS,PCLK采用CMOS相机的输出,HS、DE根据1024x768分辨率进行计数产生),转换为DVI传输后送至后级TFP401进行图像解码还原,用示波器测量TFP401还原出来的VS,HS,以及DE信号,发现这些信号噪声很多,而还原出来的像素时钟PCLK挺好,不知道为什么?根据相关资料采取措施如下:50欧并联端接,小电阻串联端接,差分线间接小电阻,问题依然无法解决,希望高手给些建议!!!
后端采用的是TFP401还是TFP401A?建议使用TFP401A,内部集成了附加电路(类似于去除抖动电路)产生更加稳定的HS,VS信号。
您这里的指的噪声很有可能是前级引入的,因此建议后端采用TFP401A来滤除这些不必要的噪音。