This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410输出视频后级TFP401无法解码还原!

Other Parts Discussed in Thread: TFP401, TFP401A

前端CMOS相机输出1412x876 50hz的视频,经过FPGA产生1024x768 50HZ视频(VS,PCLK采用CMOS相机的输出,HS、DE根据1024x768分辨率进行计数产生),转换为DVI传输后送至后级TFP401进行图像解码还原,用示波器测量TFP401还原出来的VS,HS,以及DE信号,发现这些信号噪声很多,而还原出来的像素时钟PCLK挺好,不知道为什么?根据相关资料采取措施如下:50欧并联端接,小电阻串联端接,差分线间接小电阻,问题依然无法解决,希望高手给些建议!!!

  • 后端采用的是TFP401还是TFP401A?建议使用TFP401A,内部集成了附加电路(类似于去除抖动电路)产生更加稳定的HS,VS信号。

    您这里的指的噪声很有可能是前级引入的,因此建议后端采用TFP401A来滤除这些不必要的噪音。

  • 后端采用的是TFP401,用示波器看了前端信号很干净,感觉解不出来,好像与VS,HS以及DE的时序有关系,今天改了改时序,VS和HS解出来了(HS与输入信号反向了,百思不得其解呀!),但DE信号低电平期间还有好多噪声,谁有VS,HS,DE的时序要求,不胜感激!!!我感觉DVI编码时在DE=1时对像素数据进行编码,在DE=0期间对VS,HS进行编码,所以只要DE低电平能够包住VS,HS即可,不知道这样想对不对???

  • 时序上您的理解是正确的,DE为=1时,数据编码,当为=0 时,对HS,VS编码。我这里有一份DVI1.0d的协议,在Figure 3-7有时序图,可以参考下。

  • HS解出来后极性和输入的反向了,DE信号解出来高电平还好,低电平有毛刺,望专家给予解释。分析下哪里出问题了???