This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SN65MLVD206B datasheet中描述的理解

Other Parts Discussed in Thread: SN65MLVD206B

hello ,

        在SN65MLVD206B的datasheet中有一个句话:

        Low-Voltage Differential 30-Ω to 55-Ω Line Drivers
         and Receivers for Signaling Rates
(1) Up to  200 Mbps, Clock Frequencies up to 100 MHz。

       另外关于MLVDS 有一句描述是:M-LVDS芯片可以用于速度高达125MHz的时钟和同步信号分配,也能用于速度高达250Mbps的数据和控制信号。

       个人感觉是同一个意思但是具体是什么意思呢?