This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB921&925

有一个应用,是 主机RGB信号---DS90UB921---DS90UB924---屏,现在要做一个信号源代替主机端,因为DS90UB921目前已停产很难买到,所以用DS90UB925代替,硬件上只有三个引脚有差异,目前硬件电路连接都没问题了,RGB信号也给到DS90UB925,但是屏端没有任何显示,确认DS90UB924---屏是正常的,因为对这部分不熟悉,所以在这里想请教TI的技术工程师或者熟悉这个芯片的大能,能否简单介绍一下这个串行器和解串器在上电时的通讯机制,和I2C是否需要配置?如何配置?  先谢谢了

  • 上电时的通讯机制指的是什么?上电时需要先保证上电时序的要求。

    另外,DS90UB921是一款新品,并未停产。 

    在未替代921之前,屏能正常显示吗?先确定925的输出信号是否正常。

  • 感谢你的回复

    TI的代理说 921很难拿到样品,而且价格很高。推荐我们用925

    我想请问的是,I2C如果软件不配置,只是硬件配置,是否可以正常输出信号?RGB信号是确定给到925了,但是如何测试925是否正常?屏跟主机连接的时候是显示正常的,我们现在做的是代替主机,输出RGB信号给925,再通过LVDS传给屏端的DS90UB924,驱动屏显示。