Other Parts Discussed in Thread: LMX2594
官方datasheet上说可以通过调节输出分频器的值输出10MHz到15GHz的任何频率,但其分频只能限于2/4/6/8/12/16……等,而且VCO频率大于10GHz时,最大分频值只能为6,那么其中间必然有些段落不连续, Table 8 中Channel Divider Segments表里也明确了输出不连续,为何手册上还要写科输出10MHz到15GHz的任何频率?官方不能诚实一点吗?还是该怎么理解?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We can support 900MHz, we have revised the table as below and the new datasheet will be available in ti.com very soon.
|
Div |
Min |
Max |
Max VCO |
|
1 |
7500 |
15000 |
15 GHz |
|
2 |
3750 |
7500 |
|
|
4 |
1875 |
3750 |
|
|
6 |
1250 |
2500 |
|
|
8 |
937.5 |
1437.50 |
11.5 GHz |
|
12 |
625 |
958.33 |
|
|
16 |
468.75 |
718.75 |
|
|
24 |
312.5 |
479.17 |
|
|
32 |
234.375 |
359.38 |
|
|
48 |
156.25 |
239.58 |
|
|
64 |
117.1875 |
179.69 |
|
|
128 |
58.59375 |
89.84 |
|
|
192 |
39.0625 |
59.90 |
|
|
256 |
29.29688 |
44.92 |
|
|
384 |
19.53125 |
29.95 |
|
|
512 |
14.64844 |
22.46 |
|
|
768 |
9.765625 |
14.97 |
我个人的理解是,不仅仅是这款时钟芯片,对于任何一款时钟芯片来说,即使给出了输出频率的范围,但是我们实际在进行选型时,除了根据自己的输入输出频率是否满足,还需要考虑VCO的范围,分频系数的设定,包含整数或小数等等,从而决定是否满足实际应用,不会想当然的就认为给出了一个输出频率范围,就草率的决定这款是否符合。