This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571中,部分未使用的引脚应作如何处理?

如果不使用外部VCO,也就是“合成器模式”(synthesizer mode)。

引脚30:CPoutExt,我使用内置的VCO。

引脚24:Fin,我使用内置VCO,手册载明是Open or AC coupled to GND,交流耦合到地的话多大电容?或者NC就行?

引脚28、29:FLout1、FLout2。我使用内置VCO,这两个引脚还有什么用吗?如果无用应该如何处理?

此外,

VcpExt在合成器模式下,手册指明可以接3.3或5V,我两种电源都有,接入哪一种比较好?或者没什么区别?

感谢辛勤的TI工作人员!