Other Parts Discussed in Thread: TXB0108, TXB0104, SN74LVC8T245
TXB0108在Vcca=2.5V,Vccb=3.3V的情况下允许的最大数据数率为100Mbps,如果是100Mbps时每个bit理论的最大pulse duration才10ns,但是datasheet要求是最小为10ns,这个如何达到?或者输入数据为100Mbps时会存在问题?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TXB0108对输入信号有要求,在datasheet中有这么一句话:For proper operation, the device driving the data I/Os of the TXB0108 must have drive strength of at least ±2 mA.
TXS0108最大data rate达不到100Mbps,最大60Mbps(push pull应用)。 是不是芯片本身的问题,或者你申请下免费样片重新验证一下:
http://www.ti.com.cn/product/cn/txb0108
同时,将你的电路传上来看下,如果TXB0108外围有其他电路,建议先断开其他部分,直接验证TXB0108的输入输出情况。