This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925和DS90UB940使用疑问

目前准备使用DS90UB925和DS90UB940做一套数字的行车记录显示产品,目前遇到一些几个疑问?

1、在DS90UB925的前面视频信号为YuV422I或者YC16不知道是否可以?看规格书只写了RGB888?

2、DS90UB925是720P的产品,而DS90UB940是1080P的产品,这样匹配,DS90UB940这端的寄存器设置有什么注意的地方吗?是否也要将DS90UB940设置成720P。

3、调试的寄存器配置只有这个吗?还有其他寄存器吗?

  • 1.支持。The High Speed Forward Channel (HS_FC) is composed of 35 bits of data containing DIN[23:0] or RGB[7:0] orYUV data, sync signals, I2C, and I2S audio t ransmitted from Serializer to Deserializer。

    2.925+940搭配的话,也就是说最大分辨率只能到720p。 寄存器不能配置分辨率,pixel时钟的大小决定了分辨率的大小。925的像素时钟最大85Mhz决定了支持720p的分辨率 。

    3. 调试的寄存器指的是什么?

  • 1、如果支持YuV422I或者YC16,那么剩余的不用的输入线怎么处理?悬空?还是上拉?YuV422I只有8线,YC16有16线,而925的输入有24线?
    2、925这边设置成720P后,那940这边也怎么处理?
    3、DS90UB925中的TEST pattern 寄存器只有2个(0X64,0X65) 是否还有其他寄存器可以进行测试?
    4、DS90UB940规格书里面的IFMT/OFMT意思?

  • 1. 不用的引脚可直接悬空。
    2. 925这边配置成720P的话,940这边无需做任何动作,可以自动检测。
    3. 有关test pattern的寄存器配置,建议您参考这篇应用手册:www.ti.com/.../snla132c.pdf
    4. IFMT和OFMT指的是input 和output 数据格式format。
  • 1. 不用的引脚可直接悬空。
    2. 925这边配置成720P的话,940这边无需做任何动作,可以自动检测。
    3. 有关test pattern的寄存器配置,建议您参考这篇应用手册:www.ti.com/.../snla132c.pdf
    4. IFMT和OFMT指的是input 和output 数据格式format。