This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90ub947 to Ds90ub948 高温80度屏闪问题



Hi TiTeam,

        请帮忙看看以下是否有其他问题引起的?

问题点:6台中有3台在72度左右温度升高过程中有出现过3台闪屏1次,2 次情况。升到80度时,没有太发现闪屏现象(实际测试产品机内温度为87度左右)

         确认时,闪屏出现时Ub948 Lock Pin有下掉现象,换一颗新的DS90ub948就看不到高温问题。

        根据TI提供的更改ub947寄存器

现改寄存器后碰到的问题如下:

          1,高温下现象一样,共测试4pcs

           2,亮屏后开机动画会概率有一次抖动。之前是不会有的。

我发现有抖动的话寄存器的值会跳变到,且只会出现一次。
[ 25.403596] 947 register = 0x40 read value = 0x14
[ 25.423555] 947 register = 0x41 read value = 0x55
[ 25.447194] 947 register = 0x42 read value = 0x00
没抖动寄存器的值就一直是最后写入的
[ 25.403596] 947 register = 0x40 read value = 0x10
[ 25.423555] 947 register = 0x41 read value = 0x49
[ 25.447194] 947 register = 0x42 read value = 0x00

  • 您好,

    请问您说的概率性抖动,这个概率大概是多少? 是否只发生在特定的温度呢? 另外是否有TI原厂的FAE对您进行客户支持?
  • 您好,6台中有三台闪屏,那这三台和其他三台的测试环境,都一样的吧?
    这种概率性的问题,确实不好确定问题根源,比如测试环境,系统原因等。
    三台闪屏的芯片是否有重新更换过?thermal pad 有正确处理吗?At least 9 thermal vias are necessary from the device center DAP to the ground plane. They connect the device ground to the PCB ground plane, as well as conduct heat from the exposed pad of the package to the PCB ground plane。