This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS442设计问题

Other Parts Discussed in Thread: TMDS442

HI你好,

TMDS442在single link应用中,例如从上往下输入:HDMI1,HDMI2,HDMI3,HDMI4;输出从上往下输出:PORT1,PORT2;

PORT1通过选择引脚可以输出HDMI1 or HDMI2 or HDMI3 or HDMI4?

PORT2通过选择引脚可以输出HDMI1 or HDMI2 or HDMI3 or HDMI4?

其中PORT1和PPORT2可以输出同样的输入源吗,例如:PORT1输出HDMI1,PORT2输出HDMI1?

也就是说,TMDS可以做4*2的矩阵切换吗?

另外,可否提供参考设计原理图,万分感谢!