This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI你好,
TMDS442在single link应用中,例如从上往下输入:HDMI1,HDMI2,HDMI3,HDMI4;输出从上往下输出:PORT1,PORT2;
PORT1通过选择引脚可以输出HDMI1 or HDMI2 or HDMI3 or HDMI4?
PORT2通过选择引脚可以输出HDMI1 or HDMI2 or HDMI3 or HDMI4?
其中PORT1和PPORT2可以输出同样的输入源吗,例如:PORT1输出HDMI1,PORT2输出HDMI1?
也就是说,TMDS可以做4*2的矩阵切换吗?
另外,可否提供参考设计原理图,万分感谢!