This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助CDCM7005EVM-CVAL中VCXO的产品型号

Other Parts Discussed in Thread: CDCM7005EVM-CVAL, CDCM7005

CDCM7005EVM-CVAL开发板进行测试时,发现如下的问题,请帮助解答。

       1.在开发板上的跳线棒,以及SPI软件设置均为默认设置,电源电压3.3v的前提下,PRI_REF输入端只有输入61.44MHZ频率的时候,芯片才能锁定。其他频率例如30.72MHZ,80MHZ均为失锁状态。

       2.在开发板上的跳线棒,以及SPI软件设置均为默认设置,电源电压3.3v的前提下,.PRI_REF不论端入频率为多少,输出始终保持61.44MHZ不变。

       3.这种情况我们怀疑是开发板上的片外VCXO出现了问题,对VCXO进行了测试。测试结果是随着输入频率的从小到大的变化,VCXO的V_CTRL端的电压会随着变化,但VCXO的输出端OUT的频率始终保持在491.52左右不会变化,测试结果如下:

            PRI_REF        V_CTRL      OUT(VCXO)

            30.72MHZ        66mv       491MHZ

            40MHZ           140mv      491MHZ

            50MHZ           290mv      491MHZ

            60MHZ           450mv      492MHZ

            61.44MHZ        1.65v      492MHZ 

            70MHZ           3.1v       492MHZ

       我们得出的初步结论是VCXO的频率是固定的491.52MHZ,不受V_CTRL的调节,想要咨询的问题如下:

       1.这个VCXO的频率是否是德州仪器厂家出厂前已经设置好的,不可变的,为固定的491.52MHZ

       2.如果不是设定为不可变的,是否是这个VCXO已经损坏。

       3.如果可以判定已经损坏请提供一下这个VCXO压控震荡器的型号,因为在开发板上这个VCXO上只打印了XPRESS0的字样没有具体型号。

  • CDCM7005EVM-CVAL这套EVM板的EVM user's guide中没有BOM表格。
    在CDCM7005 的其他两套demo 给出了型号为491.52Mhz的Toyocom VCXO.

    User's guide中的描述The VCXO installed on the EVM is approximately 491.52 MHz。因为我手头上暂时没有这块demo,我认为是固定的491.52MHz的VCXO。
  • 如果是这个EVM板上的VCXO只有一个固定频率的话,如果我们想测不同频率下CDCM7005的功能和相位噪声要怎么操作?您这边有相应的开发板嘛或相应的VCXO可以替换嘛,麻烦您给些建议。谢谢。

     您提到的这个User's guide中的描述The VCXO installed on the EVM is approximately 491.52 MHz,我看到过,他说的是VCXO的中心频率在491.52MHZ,而不是只有这一个固定频率,他的频率应该会随电压变化的,所以是压控振荡器。您还提到了Toyocom VCXO,我可以理解EVM板上的VCXO是Toyocom 这个厂家的吗