Other Parts Discussed in Thread: CDCM7005EVM-CVAL, CDCM7005
CDCM7005EVM-CVAL开发板进行测试时,发现如下的问题,请帮助解答。
1.在开发板上的跳线棒,以及SPI软件设置均为默认设置,电源电压3.3v的前提下,PRI_REF输入端只有输入61.44MHZ频率的时候,芯片才能锁定。其他频率例如30.72MHZ,80MHZ均为失锁状态。
2.在开发板上的跳线棒,以及SPI软件设置均为默认设置,电源电压3.3v的前提下,.PRI_REF不论端入频率为多少,输出始终保持61.44MHZ不变。
3.这种情况我们怀疑是开发板上的片外VCXO出现了问题,对VCXO进行了测试。测试结果是随着输入频率的从小到大的变化,VCXO的V_CTRL端的电压会随着变化,但VCXO的输出端OUT的频率始终保持在491.52左右不会变化,测试结果如下:
PRI_REF V_CTRL OUT(VCXO)
30.72MHZ 66mv 491MHZ
40MHZ 140mv 491MHZ
50MHZ 290mv 491MHZ
60MHZ 450mv 492MHZ
61.44MHZ 1.65v 492MHZ
70MHZ 3.1v 492MHZ
我们得出的初步结论是VCXO的频率是固定的491.52MHZ,不受V_CTRL的调节,想要咨询的问题如下:
1.这个VCXO的频率是否是德州仪器厂家出厂前已经设置好的,不可变的,为固定的491.52MHZ
2.如果不是设定为不可变的,是否是这个VCXO已经损坏。
3.如果可以判定已经损坏请提供一下这个VCXO压控震荡器的型号,因为在开发板上这个VCXO上只打印了XPRESS0的字样没有具体型号。