This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考DS90UB934EVM的设计,硬件配置:
4:OSS_SEL 10 kohm 接VDDIO。
5:OEN 10K ohm 接VDDIO。
6:BISTEN 0ohm接地。(BIST测试通过寄存器0xB3控制)
37:MODE 10K ohm接VDD1V8。
43:RES 0 ohm接地。
44:RE S 0 ohm接地。
46:SEL 0 ohm 接地。
寄存器配置:
寄存器地址 |
寄存器值 |
0x4C |
0x01 |
0x58 |
0x58 |
0x5D |
0x60 |
0x65 |
0x68 |
并行数据输出和行/场信号输出都是低,PCLK输出96MHz。
配置寄存器0xB3为0x43后进行测试,PCLK输出51.4MHz,并行数据输出和行/场信号输出都是25.7MHz,Lock和Pass为高。
还有哪里需要配置的?