This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB934 无输出



参考DS90UB934EVM的设计,硬件配置:

4:OSS_SEL 10 kohm 接VDDIO。

5:OEN 10K ohm 接VDDIO。

6:BISTEN 0ohm接地。(BIST测试通过寄存器0xB3控制)

37:MODE 10K ohm接VDD1V8。

43:RES 0 ohm接地。

44:RE S 0 ohm接地。

46:SEL 0 ohm 接地。

 

寄存器配置:

寄存器地址

寄存器值

0x4C

0x01

0x58

0x58

0x5D

0x60

0x65

0x68

并行数据输出和行/场信号输出都是低,PCLK输出96MHz。

配置寄存器0xB3为0x43后进行测试,PCLK输出51.4MHz,并行数据输出和行/场信号输出都是25.7MHz,Lock和Pass为高。

 还有哪里需要配置的?