This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10002 按照datasheet P66 1:1Mode配置,高速HSTXA和低速OUTA都无眼图

Other Parts Discussed in Thread: TLK10002

您好!

        使用贵司TLK10002,按照datasheet P66配置,通过误码仪分别向INA和HSRXA输入4.9152Gbps PRBS31或PRBS7信号,分别测试OUTA和HSTXA,都无眼图。

        1 引脚Refclk_sel=1(选择Refclk1 122.88MHz作为参考时钟),引脚Refclk0通过100欧电阻接地。

        2 可以正常读写寄存器。寄存器除0x01=0x3302(HSTX&HSRX选择1:1模式,选择Refclk1作为参考时钟),0x03=0xA545(HSRATETX和HSRATERX选择半速),0x06=0x1119(选择Lane0,LS_MPY选择20X,)外,其他寄存器配置采用各寄存器的默认值。

      请问:

       1 请问寄存器配置没有问题吧?

        2 TLK外围引脚配置还有其他注意事项吗?

        3 通过误码仪向TLK10002  INA和HSRXA输入PRBS31或PRBS7信号,在OUTA和HSTXA测试眼图,该种测试方法可行吗?

谢谢。

x 出现错误。请重试或与管理员联系。