This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

产生一个频率为30MHz和功率为6~8W的正弦波信号的需求量大产品的元件选型的问题

Other Parts Discussed in Thread: THS3122, BUF634, OPA564

大家好!请各位大神们帮忙解答以下问题,非常感谢!

我们公司的一个产品要求产生一个频率为30MHz和功率为6~8W的正弦波信号去驱动一个感性负载,各位有哪些精度高和成本低些的方案和几种不同功能的元件选型参考?

其感性负载的测试数据如下:

具体要求如下:

1)时钟芯片:能产生30MHz正弦波,精度0.1MHz,范围29.00MHz至31.00MHz。该装置需输出正弦波形稳定,无变形毛刺少,输出频率恒定;

2)高频功率运算放大器:将以上的30MHz的正弦波信号进行放大,波形基本不失真;

3)升压电路:因供电采用聚合物锂电池,电压范围为3.3-4.2V,需要升压芯片给高频运放供电,最终输出6-8W的功率;可参考输出有效电压30V-36V,输出电流200多mA,可以是这个电压和电流,也可以其它的电压和电流,只要最终输出的功率为6-8W即可。

4)在满足以上要求的前提下,这此是用于消费电子产品需求量大,芯片封装尽量容易散热,总成本尽量低些;

  • 现在已经有30MHz的精确的正弦波,但空载和频率为30MHz时的正弦波的振幅只有200mV,目前要解决将微弱的30MHz,200mV(0.2V)的正弦波信号放大到6~8W:


    初步设想目前微弱信号的频率带宽已经有30MHz,如果直接用高频运放放大信号成本很高,所以,然后先将放大器(用升压芯片给放大器供电)将电压放大到30V-36V,再将电流放大到200mA。

    请教大神们有什么好的电路或者元件选型?万分感谢!

  • 您好,这样的运放芯片不好选,首先30Mhz ,0.2V的信号放大到30~36V的话,需要运放的增益带宽积非常高,并且运放的压摆率也要高,因此从这点考虑的话可以考虑电流反馈运放, 看了几款高电流输出的电流反馈运放,比如THS3122,也无法实现输出6W功率。即使后端再使用buffer来增加驱动,比如OPA564, BUF634这类power amplifier或者buffer的GBW 收到限制,也是无法满足的呢。
  • 感谢楼上回复!是的!之前我也是这样考虑的!

    现在想能否将30Mhz ,0.2V的正弦波信号先通过ADC驱动器芯片将电流信号转换为电压信号,然后再通过一个运放放大电压到30~36V,最后通过一个电流放大器(运放)放大电流到200mA,后面的两个运放用一个升压芯片将锂电池电压升高并供电,这样就整个放大电路部分用了3个芯片,感觉复杂了些?有没有用2个芯片能解决的?或者3个芯片哪些性价比高点?请帮忙分析,非常感谢!