This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964的I2C无法访问,芯片似乎没有工作

各位专家:

我们新作的964的板卡,I2C一直无法工作,示波器测试一直都为地点平,请问大概是什么原因? MPU使用i2cdetect始终探测不到,964芯片似乎没有工作。

下边的列表是964管脚上的相关测试电压,请各位专家给些建议,到底是什么原因造成的。

      13pin   vddl_1v1   1.092v
      44pin vddl_1v1    1.093v
      21pin   vdd_csi0  1.094v
      33pin vdd_csi1     1.094v
      52pin   VDD_fpd1  1.093v
      61pin    VDD_fpd2  1.094v
      48pin    VDD18_p0  1.772v
      47pin     VDD18_p1   1.772v
      1pin       VDD18_p3   1.771v
      2pin     VDD18_p2    1.771v
      32pin    VDD18A    1.771V
      49PIN      VDD18_fpd0 1.767v
      55PN        VDD18_fpd1  1.767v
      58PIN   VDD18_fpd2 1.767v
      64PIN   VDD18_fpd3 1.767v
       16pin   VDDID      3.27V
      46PIN   IDX   1.767V
      3PIN     PDB  2.64V
      45PIN    MODE  1.771V
      4PIN    TESTEN 1.473V
谢谢各位