This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208无法锁定,配置如下,请帮忙看看什么问题?

Other Parts Discussed in Thread: CDCM6208

  1.  电源是2.5V和3.3V,测试结果分别为:2.5V和3.3V,纹波是50mV和470mV;

  2. 输入的时钟为100M,测试点为C631和C632;

  3. 更换过环路滤波电路的电容和电阻,主要是R327、C564和C560;

  4. 更换过芯片;

  5. 输出时钟

    测试125M,测试点为120M左右,测试点为芯片的14和15脚;

    测试600M,测试点为580M左右,测试点为电容C674和C675;

    测试200M,测试点为180M左右,测试点为电容R106和R116;

    测试150M,测试点为146M左右,测试点为电容R117和R225;

  6. 测试芯片的45和46脚,发现是低电平;设计原理图参照下面