附件中显示了C型电源解决方案。Type-C接口是USB3.1 GEN2 HUB的上行链路数据传输和电源接口。整个HUB解决方案需要5V 3A的电源。使用 TUSB321 作为UFP来配置CC1和CC2引脚。负载开关 TPS25910 用于控制5V VBUS电源,以防止其电流超出极限。当TUSB321 处于UFP模式时,I_MODE PIN将如何处理 ?数据表仅提到了DFP和DRP模式下的配置,如下图所示。由于HUB处于USB3.1 GEN2模式下,是否使用 TUSB321 DIR_PIN在访问后控制MUX来区分极性(由于在GEN2模式下所有的tx和rx都被利用),而DIR应该如何设计,阅读许多解决方案,使用10k电阻上拉3.3V,但在我的设计中,因为type-c接口的5V_VBUS需要通过负载开关,然后通过DC TO DC生成3V3,此解决方案无需使用emark芯片电源,如何处理FLT#_pin,此解决方案中没有MCU和其他处理器,且不想使用HUB来进行IO控制,在我的设计中ID_pin 用于使能负载开关工作,但在关于ID_pin的管脚描述中(Open drain output; asserted low when the CC pins detect device attachment when port is a source (DFP), or dual-role (DRP) acting as source (DFP).)只提到了在TUSB321作为DRP设备及DFP时的功能,在工作为UFP时,是否可以采用此引脚来控制TPS25910,希望各位工程师能给我解答一下,谢谢。(HUB控制器为VL822---USB 3.1 Gen 2 Hub Controller)