Is there a ds90ub960-q1 cascade synchronization reference solution? I want to apply a 16 channel camera. How should GPIO 0-7 connect and set up synchronization? Is there a reference schematic?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a ds90ub960-q1 cascade synchronization reference solution? I want to apply a 16 channel camera. How should GPIO 0-7 connect and set up synchronization? Is there a reference schematic?
What should I do if I use external frame synchronization? My idea is to use FPGA to generate a fixed clock signal (frame synchronization signal), connect this signal to the GPIO pin of UB960, each UB960 only needs one GPIO synchronization signal, if I use my solution, I need FPGA to output other signals To GPIO?
In addition, regarding UB960, if four UB960s are to work synchronously, do the REFCLK pins of four UB960s need the same crystal to provide the clock? Will using separate crystals affect synchronization? The data sheet says that the accuracy of synchronization is related to the accuracy of REFCLK. Is this an internal synchronization of a single UB960 using only application software? How to configure REFCLK and GPIO hardware if using 4 UB960 external frame synchronization