This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960 FPD LINK III输入RIN+和RIN-的Layout问题



我们在DS90UB960 Layout时遇到点问题需要请教一下:

1、 我们用COAX模式,FPD LINK III的输入RIN+和RIN-是否需要走差分线?960规格书中要求RIN+和RIN-要按3W原则走线,但是之前我们画933、934的PCB时,有要求走差分线。

2、 RIN-的49.9Ω端接电阻,需要靠近芯片放置,还是靠近连接器放置?

谢谢。