This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们在DS90UB960 Layout时遇到点问题需要请教一下:
1、 我们用COAX模式,FPD LINK III的输入RIN+和RIN-是否需要走差分线?960规格书中要求RIN+和RIN-要按3W原则走线,但是之前我们画933、934的PCB时,有要求走差分线。
2、 RIN-的49.9Ω端接电阻,需要靠近芯片放置,还是靠近连接器放置?
谢谢。
您好, 使用同轴电缆,RIN+和RIN-走线部分按差分信号走, 差分的阻抗是100Ohm+-10%. 在connector端, 将RIN- 端接到地, RIN+ 走50ohm单端信号.
我看datasheet中是要求走3W规则, 3W 的目的也是为了RIN+和RIN-之间的走线耦合最小,更大程度的减少串扰.