1. ULN2803在引脚输入5V时,输入电流是多少,手册中只看见3.85V时最大输入电流是1.35mA;
2. SN74HCT273的D引脚的输出电流限制是什么?手册中Continuous output current 是25mA,是单个引脚还是8个引脚之和?
3. SN74HCT273的信号引脚5V信号输入电流是多少?手册中输入电流是100uA,最大值是1mA,STM32的I/O引脚可以驱动10个CLR引脚吗?
4.根据图片连接方式,5V供电的SN74HCT273是否可以驱动ULN2803?