This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS181 I2C模式无法link up

Other Parts Discussed in Thread: TMDS181

1、两个181芯片采用pin strap模式时,HDMI接口可以link up
pin1 NC
pin10 62k电阻下拉
pin17 62k下拉
pin21和pin27 NC
pin42 上拉

2、将 FPGA  to TMDS181的这个芯片配置成i2C模式,TMDS181 TO FPGA的TMDS181保留pin strap 模式,i2c配置寄存器如附件所示,这样的环境搭建

HDMI接口不通。

问题:

a、这个问题应该如何分析,是i2c寄存器配置问题,还是硬件设计问题提?

b、FPGA TO  TMDS181方向信号链路采用DC耦合,是否需要增加上拉49.9ohm电阻?

c、两个TMDS181芯片之间的信号链路链路(中间使用线缆连接)DC耦合,是否需要增加上拉49.9ohm电阻?

TMDS181设计框图.pdf2677.I2C register dump.TXT

  • 1、两个181芯片采用pin strap模式时,HDMI接口可以link up
    pin1 NC
    pin10 62k电阻下拉
    pin17 62k下拉
    pin21和pin27 NC
    pin42 上拉

    2、将 FPGA  to TMDS181的这个芯片配置成i2C模式,TMDS181 TO FPGA的TMDS181保留pin strap 模式,i2c配置寄存器如附件所示,这样的环境搭建

    HDMI接口不通。

    问题:

    a、这个问题应该如何分析,是i2c寄存器配置问题,还是硬件设计问题提?

    b、FPGA TO  TMDS181方向信号链路采用DC耦合,是否需要增加上拉49.9ohm电阻?

    c、两个TMDS181芯片之间的信号链路链路(中间使用线缆连接)DC耦合,是否需要增加上拉49.9ohm电阻?I2C register dump.TXT

  • 您好,DC耦合不需要上拉。 TMDS to FPGA之间这里为什么使用AC耦合? TMDS181输出的也是TMDS信号, FPGA也是的话,也可以直接DC耦合。另外,source端这边的TMDS181输出是否有波形? 先测试FPGA to TMDS181这边的输出是否没问题。
    最后就是寄存器0Bh的bit1 是否合理的配置HDMI的data rate?
    0 – TMDS Clock is 1/10 of TMDS bit period (default) -> HDMI1.4

    1 – TMDS Clock is 1/40 of TMDS bit period -> HDMI2.0
  • 你好,陈工
    1、TMDS181 TO FPGA之间使用AC耦合参考一份原理图设计而成的;
    2、source端测试有时钟;
    3、0xb寄存器bit1 配置0或1都尝试过,就是不行;
    4、这个环境如果source端的TMDS181也采用pin strap模式(sink端的TMDS181一直都是pin strap模式配置),1080P、 4K@30HZ都能linkup,因此个人认为有可能是I2C mode配置的问题,请帮忙分析一下寄存器配置有什么要求?