使用PCA9534的过程中,一直都是P0-P7全部配置成输入,或者配置成输出。现在想把P0-P3配置成输入,P4-P7配置成输出,以前从来没这样操作过,查看datasheet,好像也没这方面的说明,所以发个贴问一下IT专家们,是否可以这样操作,另外这样操作了,对P0-P3作为输入,P4-P7作为成输出,彼此之间的操作是否相互独立,不相互影响,P0-P3输入反转的时候,INT正常输出;P4-P7改变输出的时候,正常写入即可。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用PCA9534的过程中,一直都是P0-P7全部配置成输入,或者配置成输出。现在想把P0-P3配置成输入,P4-P7配置成输出,以前从来没这样操作过,查看datasheet,好像也没这方面的说明,所以发个贴问一下IT专家们,是否可以这样操作,另外这样操作了,对P0-P3作为输入,P4-P7作为成输出,彼此之间的操作是否相互独立,不相互影响,P0-P3输入反转的时候,INT正常输出;P4-P7改变输出的时候,正常写入即可。
进入中断后,可以先处理中断事务,处理完之后返回来再继续执行
主要是我在PCA9534数据手册9.2.3 Interrupt Output (INT)看到“Interrupts that occur during the ACK or NACK clock pulse can be lost (or be very short) due to the resetting of the interrupt during this pulse.”:在ACK或NACK脉冲期间发生的中断可能会由于在该脉冲期间中断的重置而丢失
我看了几个其他I2C I/O扩展器都有这个缺陷,但TCA7408 可以"At no point is a valid interrupt ever missed",但TCA7408 好像已停产