我用了LMK04828芯片,仅用到了时钟同步功能,未使用PLL,因此芯片43/44引脚的参考时钟悬空未接。
输入时钟是LVDS电平,在CLKIN0、CLKIN1都接有时钟,输出配置使用TICS,将CLKIN1配置为FIN,在开发板上输出正常,但在我自己的电路板上输出接口一直无任何波形输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用了LMK04828芯片,仅用到了时钟同步功能,未使用PLL,因此芯片43/44引脚的参考时钟悬空未接。
输入时钟是LVDS电平,在CLKIN0、CLKIN1都接有时钟,输出配置使用TICS,将CLKIN1配置为FIN,在开发板上输出正常,但在我自己的电路板上输出接口一直无任何波形输出。
您好!这是我们的配置文件
R0 (INIT) 0x000090 R0 0x000000 R2 0x000200 R3 0x000306 R4 0x0004D0 R5 0x00055B R6 0x000600 R12 0x000C51 R13 0x000D04 R256 0x010001 R257 0x010155 R258 0x010255 R259 0x010302 R260 0x010400 R261 0x010502 R262 0x0106D0 R263 0x010710 R264 0x010801 R265 0x010955 R266 0x010A55 R267 0x010B02 R268 0x010C00 R269 0x010D12 R270 0x010E70 R271 0x010F10 R272 0x011001 R273 0x011155 R274 0x011255 R275 0x011302 R276 0x011400 R277 0x011512 R278 0x011670 R279 0x011710 R280 0x011801 R281 0x011955 R282 0x011A55 R283 0x011B00 R284 0x011C20 R285 0x011D12 R286 0x011E78 R287 0x011F17 R288 0x012001 R289 0x012155 R290 0x012255 R291 0x012300 R292 0x012420 R293 0x012512 R294 0x012678 R295 0x012717 R296 0x012801 R297 0x012955 R298 0x012A55 R299 0x012B02 R300 0x012C00 R301 0x012D12 R302 0x012EF8 R303 0x012F11 R304 0x013001 R305 0x013155 R306 0x013255 R307 0x013300 R308 0x013420 R309 0x013511 R310 0x013678 R311 0x013717 R312 0x013845 R313 0x013900 R314 0x013A00 R315 0x013B01 R316 0x013C00 R317 0x013D00 R318 0x013E03 R319 0x013F06 R320 0x014080 R321 0x014100 R322 0x014200 R323 0x0143D1 R324 0x014400 R325 0x01457F R326 0x014608 R327 0x014713 R328 0x014802 R329 0x014942 R330 0x014A02 R331 0x014B16 R332 0x014C00 R333 0x014D00 R334 0x014EC0 R335 0x014F7F R336 0x015003 R337 0x015102 R338 0x015200 R339 0x015300 R340 0x015402 R341 0x015500 R342 0x01560A R343 0x015700 R344 0x015801 R345 0x015900 R346 0x015A0A R347 0x015BD4 R348 0x015C20 R349 0x015D00 R350 0x015E00 R351 0x015F0B R352 0x016000 R353 0x016101 R354 0x016224 R355 0x016300 R356 0x016400 R357 0x016509 R369 0x0171AA R370 0x017202 R380 0x017C15 R381 0x017D33 R358 0x016600 R359 0x016700 R360 0x016801 R361 0x016959 R362 0x016A20 R363 0x016B00 R364 0x016C00 R365 0x016D00 R366 0x016E13 R371 0x017320 R386 0x018200 R387 0x018300 R388 0x018400 R389 0x018500 R392 0x018800 R393 0x018900 R394 0x018A00 R395 0x018B00 R8189 0x1FFD00 R8190 0x1FFE00 R8191 0x1FFF53
陈老师您好,PLL在配置软件中勾选了PD选项,对应需求的输出通道也均已打开,具体通道配置和tcs已添加附件,劳烦再帮忙确认下是否哪里配置不当,另外如果可以的话,能否麻烦您私下联系电话跟你直接请教一下,麻烦您了,感谢。