This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
1.PCA9555供电3.3V,做输入,用来监控BTS723的ST脚(开漏输出,低电平有效),测试时发现输入有效状态时刻PCA9555输出端无信号变化(两者信号未串电阻)。
2.撇开BTS723和外围,直接短路PCA9555的信号输入脚和地,能监测到输入信号正常变化,用10K电阻短接PCA9555的输入脚和地,却未能监测到输入信号,按datasheet 3.3V供电电平<0.99即认为是低电平,而10K和PCA9555和内部100K上拉算下来也只有0.3V,在低电平范围内,想问下为什么会监测不到?