This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于PCA9555的输入问题。

Other Parts Discussed in Thread: PCA9555

您好:

1.PCA9555供电3.3V,做输入,用来监控BTS723的ST脚(开漏输出,低电平有效),测试时发现输入有效状态时刻PCA9555输出端无信号变化(两者信号未串电阻)。

2.撇开BTS723和外围,直接短路PCA9555的信号输入脚和地,能监测到输入信号正常变化,用10K电阻短接PCA9555的输入脚和地,却未能监测到输入信号,按datasheet  3.3V供电电平<0.99即认为是低电平,而10K和PCA9555和内部100K上拉算下来也只有0.3V,在低电平范围内,想问下为什么会监测不到?

  • 您好,
    BTS723的ST脚OD输出外接上拉了吗
    输入低电平异常时,您有实测PCA9555输入管脚电平电压吗,实测低电平电压是多少
  • BTS723硬件电路未接上拉,ST脚直连至9555的输入脚,BTS723芯片内部串有850Ω+12K上拉,试着将11脚接的3.3V断开,现象一样,低电平拉不下来(只能拉至3.2V左右)。

    1.而单独测试BTS723,甩开9555,ST脚再上拉10K到3.3V,验证输出异常时ST脚能拉低,723开漏拉低能力应该时没问题。

    2.还有,9555的输入通过10K到地,监测不到输入信号,这个现象应该也不正常吧?我在想是否有误打开9555输出推挽的上管的可能性。

  • 1、您上传的图片没有显示,请使用回复对话框右下角“使用高级编辑器编辑文本”上传图片
    2、您可以实测一下在PCA9555与BTS723正常连接时,PCA9555输入端口的电平吗?
    您还可以实测一下当PCA9555输入端口通过10K电阻连接至地时,PCA9555输入端口的电平吗?
    我想看一下PCA9555不能识别时,其输入端口的实际电平是多少