This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVDA1040A-Q1: SN65HVDA1040A能够替代TJA1042吗?

Part Number: SN65HVDA1040A-Q1


 Hi 请教下,

SN65HVDA1040A-Q1  能够替代TJA1042吗?

SN65HVDA1040A-Q1  符合SAE J2284吗?spec里面没有看到。

  • 您好,这个是NXP 的TJA1042 和TJA1040以及和TI的两款pin to pin兼容的CAN收发器的电气参数对比。 可以看到SN65HVDA1040A-Q1 和HVDA533 都可以进行替代,但是更推荐HVDA533, 这是一款比较新的产品,相对来说它内部集成了浪涌保护以及ESD保护电路,所以外部电路不需要再加二极管保护电路。 

      TI TI NXP NXP
         
      HVDA553 HVDA1040A TJA1040U/T TJA1042T 
    Part Information        
    Status Active Active Active Active
    CAN Spec Referred ISO-11898-2 & -5 ISO-11898-2 & -5 ISO-11898-5 ISO 11898-2 & -5
    Sub-Category 5V, Single, High Speed  5V, Single, High Speed  5V, Single, High Speed  5V, Single, High Speed
    Maximum Signaling Rate 1 MBPS 1 MBPS 1 MBPS 1 MBPS
    Supply Voltage(s)        
    Vcc Pin Absolute (Min to Max) -0.3 to +6.0 -0.3 to +6.0 -0.3 to +6.0 -0.3 to 7.0
    Vcc Pin Operating (Min to Max) 4.68 to 5.33 4.75 to 5.25 4.75 to 5.25 4.5 to 5.5
    VIO / Vs Pin Absolute (Min to Max)  N/A N/A N/A N/A
    VIO / Vs Pin Operation (Min to Max) N/A N/A N/A N/A
    Thermal Information        
    Operating free-air temperature, TA (°C) -40 to +125 -40 to +125 Not Listed -40 to +150
    Junction Temp Tj (°C) (Min to Max) -40 to +150 -40 to +150 -40 to +150 -40 to +150
    Theta JA (K/W) Low-K 140 140 & 290 145 & 50 145
    Theta JA (K/W) High-K 112 112 & 52 Not Listed Not Listed
    ESD Rating and Timing        
    HBM CAN Bus Pins ESD (kV) ±12 ±12 ±6 ±8
    HBM All Pins ESD (kV) ±4 ±4 ±4 ±4
    Max Loop Delay (nS) TXD to RXD Rec to Dom 230 230 255 220
    Max Loop Delay (nS) TXD to RXD Dom to Rec 230 230 255 220
    Abs Max Voltage on Bus Pins -27 to +40 -27 to +40 -27 to +40 -58 to 58
    Notes        
    Notes IO Lines set by VCC Inputs are 3.3 Volt Compatible, but MCU must be 5V tolerant inputs. U is the bare die offering
    T is the SO8 package offering
    TJA1042T with SPLIT pin; TJA1042T/3 and TJA1042TK/3 with VIO pin.
    Packaging        
    IC Package Options 8 Pin D 8 Pin D & 12-Pin DSJ SO8 & Bare Die SO8
    Pin 5 SPLIT Split Split Split
    Pin 8 STB STB STB

    STB

     

  • Hi

    我看到HVDA533的规格书是2013年的,SN65HVDA1040A-Q1规格书是2015年的,HVDA533不是应该版本更老吗?另外,这两个分别都符合SAE J2284吗?

  • 您好,HVDA533 您可能看的不是最新版本的,可以对比下,第一版本的话,HVDA533是2013,而SN65HVDA1040A是2010年,所以相对来说,HVDA533 要新一些。 关于SAE J2284, 从二者的应用来看,都是可以用于SAE J2284 High-Speed CAN for Automotive appication上。

  • Hi

    感谢回答,另外想要了解这个SAE-J2284是什么协议?TI有懂这方面的专家吗?在选型的时候不确定是否需要这个协议或要求,所以想要了解,多谢

  • SAE-J2284是高速CAN总线,汽车应用等级的一种标准。 具体协议标准很抱歉我这边没有相关资料。 

    或者您也可以在英文E2E上咨询下美国的资深工程