This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD231: CANH和CANL在Recessive状态下的电平不正常

Part Number: SN65HVD231
Other Parts Discussed in Thread: TCAN330

SN65HVD231使用3.3V供电,CAN总线上有2个节点,其中一个节点只发送数据,另外一个节点只接受数据。在发送数据的节点测量CAN差分信号,发现CANH和CANL在Recessive状态下的电平不对,正常应该为2.3V,实测只有1.9V左右。

x 出现错误。请重试或与管理员联系。