This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AD: PD IC在给电池充电的时候行为异常,VBUS电起不来

Part Number: TPS65994AD

PD IC异常问题点:
主板1 插TypeC和电池都不开机,量测+3V_LDO和+1.5V_LDO有电,I2C_IRQ#开机拉high一下后一直为Low,I2C_SDA一直在发,按Powerbutten不开机,把I2C_IRQ#断开TypeC/Battery都可以开机,但TypeC口电池充电行为异常,现象如下:
1.先插TypeC后插电池开机后能充电
2.先插电池后插TypeC开机后不能充电(TypeC完全不起电)
3.插着TypeC开机后插电池不能充电
4.插着电池开机后插TypeC不能充电(TypeC完全不起电)
5.插着电池和TypeC开关机一次,再开机就能充电
量测CC1和CC2,插着电池再插TypeC时沟通会异常(对比正常的Port)
主板2 插TypeC可以正常开机,插Battery不开机,量测+3V_LDO和+1.5V_LDO没有电,按PowerButton不开机,先把I2C2s_SDA和I2C2s_SCL的PU换成+3VSUS,最后把I2C2s_IRQ#断开,插电池可以开机。
目前的状态是I2C2s_SDA和I2C2s_SCL的PU是+3VSUS,I2C2s_IRQ#断开,插Battery和TypeC都能正常开机,但充电行为也是异常
1.先插TypeC后插电池开机后能充电
2.先插电池后插TypeC开机后不能充电(TypeC只有5V)
3.插着TypeC开机后插电池能充电,TypeC插拔一次又不能充电,此时量测TypeC只有5V
4.插着电池开机后插TypeC不能充电(TypeC只有5V)
主板3 插TypeC可以正常开机,插Battery不开机,量测+3V_LDO和+1.5V_LDO没有电,Slp_S5不起,按PowerButton不开机,把I2C2s_SDA和I2C2s_SCL的PU换成+3VSUS,然后断开I2C2s_IRQ#,插电池可以开机,充电行为异常:
1.先插TypeC后插电池开机后能充电
2.先插电池后插TypeC开机后不能充电(TypeC只有5V)
3.插着TypeC开机后插电池能充电,TypeC插拔一次又不能充电,此时量测TypeC只有5V
4.插着电池开机后插TypeC不能充电(TypeC只有5V)