This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953A-Q1: 使用问题

Part Number: DS90UB953A-Q1


我们现在的相机是5百万,30fps,但是是黑白的,我们的传感器是IMX264,分辨率是2448*2048,帧率是30FPS,因为是颜色是黑白的,所以每个像素只点8位或10位或12位。可以使用DS90UB953和DS90UB954吗?

  • 您好,可以计算一下总的data rate,按12bit,消隐15%来计算的话:

    2448*2048*30*(1+15%)*12约等于2Gbps,而MIPI 编码的最大data rate为3.2Gbps,953能支持到4.16Gbps的total data rate。

    所以计算下来是支持的。