This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想用STM32F4和DP83640实现1588时钟同步,之前从未有过类似额开发经历。我已经下载了snlu049的开发库,请问我需要将什么内容移植到STM32的工程中呢?我看ST官方提供的1588例程需要移植LWip和FreeRTOS,然后连接PYH以太网芯片,使用STM32自身硬件功能实现PTP同步。要是我使用DP83640这款自带1588功能的芯片,我该如何下手呢,有做过相关项目的大佬能解释一下吗。
您好,关于您的这个问题,我已经帮您提交到英文E2E论坛上了,美国工程师已经做出回复,您参考一下,您可以在上面直接跟进,或者这里跟进,我帮您回复也可以的:
您好,DP83640是工作在RMII master 模式还是RMII slave模式?参考时钟输入不是RXCLK,是Pin31的X1, 如果工作在slave
模式,X1 需要的是50-MHz 0.005% (±50 ppm)的输入,如果是master mode的话,需要25Mhz的参考输入。
工程师,您好!我打算使用RMII MASTER方式,但是使用RMII模式需要给STMF407输出参考时钟,但是评估板上X1引脚并没有引出来,所以我现在使用的是MII模式,并且已经能通信成功。但是,目前遇见的问题是使用STM32F407的MIC接口,通过PMODI和PDMC并不能读出DP83640芯片寄存器的值。我已经检查了程序中相关时钟这些已经配置好了,GPIO端口选择也没问题,但使用库函数读取的寄存器值返回的全是0XFFFF(例如使用这句函数读取寄存器02h的值,HAL_ETH_ReadPHYRegister(&heth, 0x02, ®ister_data);)。请问,这是什么原因呢?