This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP159: 输出720P及以下分辨率不正常

Part Number: SN75DP159

TI的工程师,你好,我在调试一个方案,TMDS IN ,HDMI OUT ,DP159缺省寄存器配置,1080P30,P60,4KP30,能出,720P及以下的分辨率出不了正常的分辨率,我更改DEC_FUNC_MODE为Automatic retimer for HDMI2.0时能出4K60了但是720P及以下的还是出不了正常的 DP159外围电路.doc

  • 您好,硬件方面,SDA/SCL_sink,SDA/SCL_SRC以及SDA/SCL_CTL都需要上拉2K到VCC。

    几个strap pin引脚的上拉建议65Kohm,下拉0~65Kohm,3.3V和1.1V电源去耦电容建议0.1uF。我看电路中都没有。

    另外,关于720p以下, 您需要计算下total data rate,DP159的data rate最低是250Mbps。720p@60fps,24bit的话,我们计算以下total data rate:

    1024*720*60*24,按15%消隐区计算的话,总的是低于250Mbps的,所以我想这是720p不能正常工作的原因。

  • 您好,硬件方面,SDA/SCL_sink,SDA/SCL_SRC以及SDA/SCL_CTL上拉到了VCC,去耦电容也有,只是没截到,还有就是您说的data rate 的计算您是怎么计算的呢,我这边计算的跟您的不对,是1280X720X60X24/0.85   算出来是1.5G了,  

    720P的有效区1280x720   总宽高1650x750

  • 哦我计算的时候没把24bit乘进去。用的1280*720*60*(1+15%)是小于250Mbps的。

    我计算错了,即使是8bit 色深,这样再乘以8,data rate也是大于250Mbps了。

  • 您好,您的问题怎么样了?

    在未改720p之前时,配置的是retimer mode还是redriver mode?

    如果您想通过DEC_FUNC_MODE更改时,需要先切换PD_EN bit,然后再去配置DEC_FUNC_MODE才会生效。

    另外DEC_FUNC_MODE改为配置10(automatic retimer HDMI2.0 mode)时,TMDS_CLOCK_RATIO_STATUS 配置了多少?