Part Number: SN65DSI86
Hi TI
我们项目使用SN65DSI86 ,用于MIPI转DP输出,做标准的DP HBR2测试是出现Fail(见附件报告DP HBR2.PDF),从报告上看SN65DSI86在做DP 测试时,不会随着trainning 的要求输出不同的电平值,是否SN65DSI86这种 VPP 或者预加重如果寄存器写了固定的值就不会改变;或者测试HBR2是需要进入特别的模式?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI86
Hi TI
我们项目使用SN65DSI86 ,用于MIPI转DP输出,做标准的DP HBR2测试是出现Fail(见附件报告DP HBR2.PDF),从报告上看SN65DSI86在做DP 测试时,不会随着trainning 的要求输出不同的电平值,是否SN65DSI86这种 VPP 或者预加重如果寄存器写了固定的值就不会改变;或者测试HBR2是需要进入特别的模式?
您好,因为我这边没有找到相关HBR2测试的相关资料。但是根据您的描述来看,首先Vod的值以及预加重的值如果通过寄存器配置,这个值应该是不会变的。
另外,测试HBR2时,寄存器0x96 bit[3:0]是否已经配置为0110 = HBR2 Compliance Eye Pattern?

您好,除了配置 DP_PRE_EMPHASIS 以及DP_TX_SWING的level之外,DP Link Training LUT regsiter是否有配置?
比如port0的配置,DP_PRE_EMPHASIS =level0,DP_TX_SWING=level 0,但是bit[3:0]这里默认的是0100=4,所以代入y公式VOD = 200 + 50 × V0_P0_VOD=400mV,如果要更改Vod,这几位也需要配置。这几位的配置最大为12=1100,所以Vod最大为800mV。 不知您是否对这几个port的寄存器是否有配置,只配置 DP_PRE_EMPHASIS 以及DP_TX_SWING的level之外,应该是不能更改Vpp的幅值的。