用 TFP401 将 HDMI 信号转换为 RGB 信号驱动2款 TFT LCD 模组,分辨率是 800*480 和 1024*600, 请问 TFP401 需要做那些设置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,不需要通过TFP401的寄存器配置分辨率。换句话说,输入给TFP401的视频源的分辨率是一定的,只需要看TFP401是否支持这个分辨率就好。
TFP401是24bit的,显示面板是多少位的?
另外,data mapping是否和panel的对应一致?比如RGB的MSB,LSB对应是否正确?

嗯 采用是1 pixel mode,那么ODD输出不需要接,奇偶像素都是在QE上传输的。
我看了下TFP401的data接的都没问题,Display这边的data mapping都没问题吧,我看下面Note好像备注的是24bit source,18bit receiver。
如果是24bit的话,要按照24bit data mapping接。
因为从显示图像来看,应该还是RGB这边接线的问题。