This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812R-Q1: 关于以太网SMII接口的问题:支持RMII的PHY芯片可以支持SMII吗?

Part Number: DP83TC812R-Q1


RMII数据位宽为2,通信频率50MHz;SMII数据位宽为1,通信频率125MHz。

SMII比RMII使用更少的连接引线。

以我理解的来看,只要PHY和集成MAC的CPU支持125MHz频率,就可以支持SMII通信,可以这样认为吗?

(我搜索了很多PHY芯片,都没有标注支持SMII接口,这是为什么呢?)

SMII接口: