Part Number: DS90UB960-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
您好,您的意思是两片960和 imX390-GW5200-TI953 camera 连接的话,视频显示是正常的。
但是一片960 和imX390-GW5200-TI953 camera 连接,会出现丢帧现象是 吗?
另外,您提到的这款imX390-GW5200-TI953 camera 是内部集成了TI953这款串行器是吗?
您好,丢帧的这种情况,也就是您只使用960的RX 的一路,因为RX有四路,960可以同时接4路953,所以接4路的时候是显示没问题的。
但是如果只接一路的话,其他几路RX不适用是需要配置为disable的,寄存器0X0C RX_PORT_CTL可以配置您使用哪路,其余不用的可以将其disable掉。
因为默认的是这四路都是enable状态的,所以当您只接其中一路时,会出现丢帧现象。