This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: matching DS90UB953 with DS90UB960-Q1

Part Number: DS90UB960-Q1


Hi Team,
 
We had some problems matching DS90UB953 with DS90UB960-Q1.
Our controller uses 2 pieces of DS90UB960-Q1 and 8 channels are connected to imX390-GW5200-TI953 camera. There is no problem and the video data is normal.
2 pieces of DS90UB960-Q1 each connected with 1 IMX390-GW5200-TI953 camera, there will be a large number of frame loss phenomenon. What causes this phenomenon?
I look forward to your reply. Thank you.
Best Regards,
sukie
  • 您好,您的意思是两片960和 imX390-GW5200-TI953 camera 连接的话,视频显示是正常的。

    但是一片960 和imX390-GW5200-TI953 camera 连接,会出现丢帧现象是 吗?

    另外,您提到的这款imX390-GW5200-TI953 camera 是内部集成了TI953这款串行器是吗? 

  • 您好:

    感谢您的回复,我们现在使用的是imX390-GW5200-TI953这款摄像头,内部集成了TI953这款串行器。LI-IMX390-GW5200-FPDLINKIII-xxxH_datasheet(1).pdf

    TI960的4个fpdlink通道,接4个imX390-GW5200-TI953摄像头,我们用了2片TI960,一共接8路摄像头,8路摄像头全接,视频显示正常。


    2片TI960,各接1路摄像头,这种情况就会有丢帧现象。

  • 您好,丢帧的这种情况,也就是您只使用960的RX 的一路,因为RX有四路,960可以同时接4路953,所以接4路的时候是显示没问题的。

    但是如果只接一路的话,其他几路RX不适用是需要配置为disable的,寄存器0X0C RX_PORT_CTL可以配置您使用哪路,其余不用的可以将其disable掉。

    因为默认的是这四路都是enable状态的,所以当您只接其中一路时,会出现丢帧现象。

  • 您好:
         非常感谢您的回复,我们的问题已解决。

    顺便咨询一下,导致这个问题的根本原因是什么?是通道之间相互干扰?