您好,
我们目前设计是屏幕端使用DS90UB948的GPIO3(pin9)引脚传输触摸屏的INT信号(触摸屏IC是GT915L),主机端使用的是DS90UB941。941的0x0f寄存器设置成0x05,948的0x1f寄存器设置成0x03。
目前测试发现触摸屏INT信号接到948之后,3.3V的电平幅度被拉低到0.8V左右,断开触摸屏INT脚和948的连接可恢复正常。参照GT915L的规格书说明,要求INT脚接收端需要配置成浮空输入的状态,所以想请问948的GPIO是否可以配置成浮空输入?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我们目前设计是屏幕端使用DS90UB948的GPIO3(pin9)引脚传输触摸屏的INT信号(触摸屏IC是GT915L),主机端使用的是DS90UB941。941的0x0f寄存器设置成0x05,948的0x1f寄存器设置成0x03。
目前测试发现触摸屏INT信号接到948之后,3.3V的电平幅度被拉低到0.8V左右,断开触摸屏INT脚和948的连接可恢复正常。参照GT915L的规格书说明,要求INT脚接收端需要配置成浮空输入的状态,所以想请问948的GPIO是否可以配置成浮空输入?
941的GPIO3是连到SOC上的,我是需要把触摸屏的INT信号发到SOC上,方向应该是触摸屏-》948-》941-》SOC。所以我现在这个配置应该没问题吧?
方向是我搞错了,您这个方向没问题;
948的GPIO3配置成输入之后,内部不应有下拉,否则就失去了输入的意义;
SOC上连接GPIO3的管脚,SOC设置的此输入状态是什么状态?是否设置成了浮空输入?
我又考虑了下,SOC那边I/O的输入配置应该不会影响,因为这经过了BCC,不会影响INT的状态;
触摸屏的INT是什么输出接口?是OD或OC输出接口吗?
寄存器 0x34[1:0]您配置的是多少?
是否可以直接将触摸屏的INT脚连接到Soc输入,看INT电平是否被拉低?
另外,寄存器写入是否验证了可以正确写入