This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: 使用GPIO引脚传输触摸屏INT信号

Part Number: DS90UB948-Q1

您好,

        我们目前设计是屏幕端使用DS90UB948的GPIO3(pin9)引脚传输触摸屏的INT信号(触摸屏IC是GT915L),主机端使用的是DS90UB941。941的0x0f寄存器设置成0x05,948的0x1f寄存器设置成0x03。

目前测试发现触摸屏INT信号接到948之后,3.3V的电平幅度被拉低到0.8V左右,断开触摸屏INT脚和948的连接可恢复正常。参照GT915L的规格书说明,要求INT脚接收端需要配置成浮空输入的状态,所以想请问948的GPIO是否可以配置成浮空输入?