This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于TLK2521问题,谢谢



你好,我这边准备利用两片TLK2521做一个通信系统,一个TLK2521作为发送数据方,另外一个作为接受数据方,传输距离7米或者10米,速率约为2Gbps/秒,接受方需具备失锁后重新锁定的功能,发送和接受方分别加TI的预加重和均衡芯片,利用FPGA对TLK2521进行控制。我有几个问题想请教一下:

1.datasheet上有两种同步方式,第一种快速同步,发送芯片发送同步码型,接受芯片对数据进行锁定。datasheet推荐解串行端的LOCKB信号直接与发送器的SYNC引脚相连。如果我使用这种方式,我是否还需要将作为接受方的那一片TLK2521的LOCKB脚连接到作为发送方的TLK2521的SYNC引脚上去?如果需要,考虑到我的传输距离,这里就需要对这根线单独做一个驱动?

2.第二种同步方式,随机锁定同步,开环或者热插拔后也能进行锁定的方式。我也希望利用这种同步方式。The deserializer stays in lock until it cannot detect the same data boundary (start/stop bits) for four consecutive
cycles. Then the deserializer goes out of lock and hunts for the new data boundary (start/stop bits). 我想知道作为接收方的TLK2521失锁之后,能否自动进行同步,还是需要将失锁的消息通知给发送方TLK2521,让其发送SYNC同步码,接受方TLK2521收到同步码后进行同步?如果是这样,第二种同步方式和第一种同步应该就是一样,都是接受方失锁后主动通知发送方,再让其发送同步码同步?也就是两种同步方式完全一样,有啥区别?

3.数据速率约为2Gbps/秒,但实际有效数据小于此数据量,也就是还需要自己做一个帧的打包和解包过程来提取数据?

4.串行数据传送的时候,速率约为2Gbps/秒,串行数据P和N极通过一对双绞线传送合理还是P和N都分别利用同轴线,与地进行绞合,而P,N不互相绞合一起这种方式合理?

5.datasheet上的PLL startup lock time,是否是发送方发送SYNC同步码后,接受方的TLK2521重新达到锁定的时间?如果是,也就意味着发送方需要等待0.4ms之后再进行发送,否则数据就会丢失?

6.我的应用中发送芯片只作为发送,接收芯片只作为接收芯片,接收芯片也必须接一个与发送芯片时钟频率差异很小的时钟?求核实

期待贵公司的回复,谢谢哈。

  • 关于你的几个问题,

    快速同步模式主要是监测LOCKB的状态来判断解串器是否对串行数据进行锁存,换句话说, 发送端并转串的数据是否已经准确无误的进入到解串通道然后对其进行串并转化。datasheet中只是给出了一种方法,我个人认为也可以不需要将LOCKB和SYNC接在一起,如果传输距离比较长,接在一起的话,考虑到传输线引起的信号失真,信号抖动,最好需要一款对信号进行调节的芯片。