你好,我这边准备利用两片TLK2521做一个通信系统,一个TLK2521作为发送数据方,另外一个作为接受数据方,传输距离7米或者10米,速率约为2Gbps/秒,接受方需具备失锁后重新锁定的功能,发送和接受方分别加TI的预加重和均衡芯片,利用FPGA对TLK2521进行控制。我有几个问题想请教一下:
1.datasheet上有两种同步方式,第一种快速同步,发送芯片发送同步码型,接受芯片对数据进行锁定。datasheet推荐解串行端的LOCKB信号直接与发送器的SYNC引脚相连。如果我使用这种方式,我是否还需要将作为接受方的那一片TLK2521的LOCKB脚连接到作为发送方的TLK2521的SYNC引脚上去?如果需要,考虑到我的传输距离,这里就需要对这根线单独做一个驱动?
2.第二种同步方式,随机锁定同步,开环或者热插拔后也能进行锁定的方式。我也希望利用这种同步方式。The deserializer stays in lock until it cannot detect the same data boundary (start/stop bits) for four consecutive
cycles. Then the deserializer goes out of lock and hunts for the new data boundary (start/stop bits). 我想知道作为接收方的TLK2521失锁之后,能否自动进行同步,还是需要将失锁的消息通知给发送方TLK2521,让其发送SYNC同步码,接受方TLK2521收到同步码后进行同步?如果是这样,第二种同步方式和第一种同步应该就是一样,都是接受方失锁后主动通知发送方,再让其发送同步码同步?也就是两种同步方式完全一样,有啥区别?
3.数据速率约为2Gbps/秒,但实际有效数据小于此数据量,也就是还需要自己做一个帧的打包和解包过程来提取数据?
4.串行数据传送的时候,速率约为2Gbps/秒,串行数据P和N极通过一对双绞线传送合理还是P和N都分别利用同轴线,与地进行绞合,而P,N不互相绞合一起这种方式合理?
5.datasheet上的PLL startup lock time,是否是发送方发送SYNC同步码后,接受方的TLK2521重新达到锁定的时间?如果是,也就意味着发送方需要等待0.4ms之后再进行发送,否则数据就会丢失?
6.我的应用中发送芯片只作为发送,接收芯片只作为接收芯片,接收芯片也必须接一个与发送芯片时钟频率差异很小的时钟?求核实
期待贵公司的回复,谢谢哈。