This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK1501: 概率性出现 RX_CLK 错位

Part Number: TLK1501


有个项目,用到了TLK1501,目前也有一个问题,不知道是哪里出了问题。方案如下:

1.我的这边作为接收端,发送端未使用,处于悬空状态(是否能悬空)?

2.时钟方案,由于发送端的时钟是35MHZ,所以TLK1501的GTX_CLK也配置为35M(有个文档说GTX_CLK时钟要随恢复出来的时钟做动态调整,是否一定需要这样做)。文档如下:

3.我方设备,有些设备可以正常接收,解出发送端设备发送的数据。有些设备 有概率性的出现解析不出数据。这个时候测试RX_CLK波形,发现有异常。

这个异常出现通常是我方设备和对方设备对接后,都上电的情况下出现的。如果我方设备单独上电,RX_CLK没有问题,频率同GTX_CLK。我方设备上电,然后给对方设备上电,概率性出现刚才描述的现象。先给对方设备上电,再给我方设备上电,也会概率性的出现问题。同时上电,也有概率性的问题。请问这个是什么原因引起的?RX_CLK测试波形如下:

4.TLK1501 供电为2.5V,RX_D0---D15、RX_ER、RX_DV 为啥是3V左右的电平.DATAsheet给出的是最大2.7V。这是为啥呢?测试波形如下:

  • 发现一个现象:CDCE62005RGZT的输出不稳定,配置27脚单端输出35M时钟输出,给到TLK1501的GTX_CLK。有时候接收端设备上电在34.72---35.21MHz间(大部分时间在34.97到35.09间跳),此时不会出问题;有时候接收端设备上电,这个时钟在35.59---35.97MHz间波动,此时给输入源端设备上电,RX_CLK 一定会出问题。源端设备的TLK1501的GTX_CLK为35MHz。

    从此现象上判断,是因为发送端和接收端的时钟频率差值超出了容限范围导致。

  • 1.您好,应用手册中给出了TLK1501的两种工作模式,一种是收发模式,一种是只发模式。没有提到只收模式,所以想和您确认下,后面几个问题都是在只收模式下测试的吗?

    有个文档说GTX_CLK时钟要随恢复出来的时钟做动态调整,是否一定需要这样做)

    2.关于第二问,这个应该是内部时钟合成模块来控制的,不需要我们外部控制。 我再看下。

    3. 不论是你这边先上电,还是对方先上电,或者同时上电,我建议都是先将TLK1501处于power down状态,即Enable 引脚为低电平,当上电都完全起来稳定之后,再将Enable拉高,看此时恢复出来的时钟是否还出现异常。

    4. VDD的供电电压最大2.7V,最小2.3V,典型值为2.5V,所以这里的2.7V应该是指的2.7V最大供电条件下的波形,如果2.5V供电的话,这里应该是2.5V。