有个项目,用到了TLK1501,目前也有一个问题,不知道是哪里出了问题。方案如下:

1.我的这边作为接收端,发送端未使用,处于悬空状态(是否能悬空)?
2.时钟方案,由于发送端的时钟是35MHZ,所以TLK1501的GTX_CLK也配置为35M(有个文档说GTX_CLK时钟要随恢复出来的时钟做动态调整,是否一定需要这样做)。文档如下:

3.我方设备,有些设备可以正常接收,解出发送端设备发送的数据。有些设备 有概率性的出现解析不出数据。这个时候测试RX_CLK波形,发现有异常。
这个异常出现通常是我方设备和对方设备对接后,都上电的情况下出现的。如果我方设备单独上电,RX_CLK没有问题,频率同GTX_CLK。我方设备上电,然后给对方设备上电,概率性出现刚才描述的现象。先给对方设备上电,再给我方设备上电,也会概率性的出现问题。同时上电,也有概率性的问题。请问这个是什么原因引起的?RX_CLK测试波形如下:

4.TLK1501 供电为2.5V,RX_D0---D15、RX_ER、RX_DV 为啥是3V左右的电平.DATAsheet给出的是最大2.7V。这是为啥呢?测试波形如下: